Part Number: ADS131E08
I am having problems with using integrated opamp. It is not producing correct signal despite being setup correctly.
config1 = 0x92
config2 = 0xE0
config3 = 0x45 (this should connect non-inverting input to OPAMPP pin and enable the opamp.)
I have verified that registers are set correctly by reading them back.
The gain of the opamp is setup to be 28. Inverting pin is connected to ground via 1k resistor. Non-inverting pin is connected to a 100 Ohm current sense resistor that drops 98mV. Output pin is connected to inverting pin via 27k resistor, which produces gain of 28. Output pin is also connected to VREFP and is meant to supply 2.744V of reference voltage.
Also, I found rather worrying thread https://e2e.ti.com/support/data-converters/f/73/t/614280, which contains no resolution.