Part Number: ADS131A02
Other Parts Discussed in Thread: ADS131A04
Hi team,
My customer uses ADS131A02 with Asynchronous Interrupt Mode and he is asking questions about DRDY behavior after RESET.
After both hardware/software reset, DRDY pin shows some periodic pulses as shown in ① and ② in this waveform which can be accessed via TI network.
- Is this expected behavior?
- Is there no possibility that DRDY sticks to High or Low after Reset?
[Background of the questions]
As I mentioned above, the customer uses the device with Asynchronous Interrupt Mode. So he designed that master controller doesn't output SLK unless IQR is interrupted. Current device setting procedure is as follows.
- Power Up
- Hardware or Software Reset
- Wait 7ms
- Output SCLK from controller once falling of DRDY is received.
- Receive READY word and send UNLOCK command
As of now, the customer uses DRDY pulse to trigger SCLK from controller and it works properly without any problem so far.
But he is concerned about if there is possibility that DRDY sticks to High or Low and controller never output SCLK because there is no description about DRDY behavior after POR on the datasheet.
Should he just output SCLK after 4.5ms from RESET w/o triggering?
Best regards,
Shota Mago