This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC7836: AMC7836 W/R Register Delay

Part Number: AMC7836

Hi Team,

Does AMC7836 needs to add delay window between each W/R register? my customer found that, after register configuration, all the register could become zero if frequently change the gate voltage setup. This can be solved if re-config the registers.

thanks a lot.

Best regards,

Yang

  • Hi Yang,

    I would be more concerned if there is some kind power/reset event being triggered.  Could they verify if all of the configuration are getting reset? If so, can they monitor the VCC/VSS/VDD supplies to see if there are glitches or transients?

    thanks,

    Paul