Part Number: DAC5662-EP
Hello,
I am interested in using the DAC5662-EP for my application. My FPGA board can provide 2.5V LVCMOS Data Bus and WRTA/B signals. Seems like it meets the minimum VIH requirement of 2V as per the datasheet. But I would like to confirm this. The DAC will be powered at 3.3V DC and all other controls + clock signals will be 3.3V CMOS levels. The Data bus and WRT/B signals are the only ones at high speed, driven directly from the FPGA at 2.5V. Kindly advise.
Regards,
AB