Part Number: ADS131M08
Hi,
I am measuring offset error for the first four-channels of ADS131M08. Global chop mode is always active and PGA is set to 32. Firstly using calibration registers I shorted ADC inputs to AGND and measured around 2µV to 15µV. Which is I think is acceptable according to the datasheet (Section 6.5 Electrical Characteristics). Now I applied 0V externally to ADC and measured around 0.005mV at the input of ADC. When I look at the output code of the ADC it is giving me 1.4mV for channel-0, 731µV for channel-1, 639µV for channel-2, 274µV for channel-3. I expected the offset error will differ from channel to channel but will remain under +-32µV because global chop mode is enabled. From my measurements that is not the case and would like to know what might be causing this behavior.
Thank You
Best Regards
Adla