Part Number: DAC11001A
Other Parts Discussed in Thread: OPA189, TINA-TI, OPA192, OPA827
Hey everyone,
For an SMU-like device that requires good DC precision and fast settling, I'm evaluating the DAC11001A from TI. I have a few questions after going through the datasheet:
1. For my application, I would like to use the built-in resistors (available through pins ROFS, RCM and RFB) to generate the negative reference voltage. What is the matching ratio of these internal resistors (typical, maximal)? Along the same lines, how well matched are they in terms of temperature drift?
2. The datasheet states for the capacitors in the feedback loop of the reference buffers, that "the values of C1 and C2 depend on the stability criteria of the reference buffers when driving the reference inputs of DACx1001. The values are obtained through simulation." How should I simulate this, e.g., using TINA-TI for the OPA192 and OPA189 op amps? Or can you perhaps recommend values for C1, C2 for these two op amps?
2. As they are already used elsewhere in the design and have excellent DC specifications, the OPA189 or OPA192 would be preferred candidates to use for the reference buffers. I noticed the OPA189 is mentioned explicitly in the datasheet. Would the OPA192 also work in this position, or would it adversely affect the performance of the DAC (apart from the slightly higher output voltage offset)?
Best regards,
Jacques