Part Number: ADS8668
Other Parts Discussed in Thread: ADS8688
Dear Technical Support Team,
My input circuit of ADS8668 is below.
Signal generator that I have makes only 0~10V. it can't make 0~-10V
So I try to input reverse connection input(AIN_0P=0V and AIN_0N=0~ - 10V), then ADS8668 looks converting correctly(0~-10V).
I understand that ADS8688 supports only single-end input.

This is PGA on datasheet. I'd like to calculate above behavior on PGA circuite.
However I don't know the PGA behavior and RDC and RFD when input range setting is ±10V.

Best Regards,
ttd