Part Number: ADS1018-Q1
What is the maximum recommended input impedance which one should connect externally to one of the ADC's input?
I can't seem to find the relevant data about it in the datasheet. I will have between 5k and 10k, max. 100Hz sampling rate and hope to get between 10 and 12 ENOB.
I don't want to just put an opamp buffer before confirming whether it is needed or not.
Thank you!