Part Number: ADS1675
Hi Sir,
When I use ads1675,the OTRA pin is connected to the ground through a resistor and LED light,
The LED lights keep flashing after the power on,
The measured input level of AINP and AINN is about 2.5V.
Even if the voltage of the DVDD is connected to 3V, the condition is not improved.
The collected output data is always jumping,
What's the matter with this, please.
Could you please share your valuable suggestions?
Thanks.
Regards,