Part Number: ADS1284
We are currently evaluating the ADS1284.
We felt that the output stability of the ADC was higher than expected, so we enabled the Internal Short feature.
However, the output stability of the ADC did not improve. Please give me some advice.
Our evaluation environment is as follows. The evaluation board is the board we designed.
AVDD: + 5V, DVDD: 3V, VREF: 1V, fclk: 2MHz, Config0: 00010010, Config1: 00101000