Part Number: ADS7038
Hi,
I have a very similar question as to that raised in this thread "Compiler: Manual and On-the-fly mode operations" There Art Kay said "1. Regarding your objective to " from time to time send a refresh command for the digital outputs". For Manual, and on-the-fly mode SDI is used to select the channel ID. For the Auto-sequence mode SDI is set low and not used. So, regardless of the mode you choose, you will need to stop converting and do a register write (24 bit write) to the GPO value register."
My question is how do you stop and start the ADC conversion in on-the-fly mode so that a register read/write can be performed? I'm unclear of what registers need to be written to stop on-the-fly mode before I can read/write to the GPIO registers, or can I just do a register read/write to GPIO and that will automatically stop on-the-fly mode?
Thanks
Simon