Part Number: ADC08D500
When we used ADC chip ADC08D500, we found that the output of ADC chip had burr and the working temperature was very high. The surface temperature was measured at 70℃ with an infrared thermometer.
After many measurements, the conclusion is as follows:
There is no burr in the ADC output when the power is turned on at low temperature. In the case of constant power supply, even if the subsequent temperature rise will not affect the ADC output.
In a high temperature environment, ADC output burr, the higher the temperature, the more burr, the subsequent use of fans to reduce the temperature can not make the ADC output better.
I would like to ask you what is the reason for this situation?Looking forward to your reply!