Part Number: ADS131M04
Hi,
I am under the design phase of my application which monitors the input current on all the phases and measures the protection featured faults to isolate the Circuit Breaker from Load.
Our Input current range for the Application varies till 8000A. But while referring the design document of this IC ADS131M04, it says that the current range is from 0.05A to 100A.
Is there any similar ICs which can be used for high current inputs?
Regards,
Raguram