Part Number: ADS7828
Dear Tom,
I would like to add more questions to this.
If the AIN of this device is not used, what Ω should be used for termination to GND ?
What should be with multiple unused analog input terminals if this circuit is fixed and does not change ?
Is it okayto short-circuit all unused terminals and terminate with a single resistor (10k ohm?) ?
Or should it be terminated for each terminal ?
Regards,
SNDS