Part Number: ADS1292
Hi TI
- When using only RA and LA without using RLD
In case of DC coupling (no use of series capacitor) RA and LA to ADS1292 and biasing with AVDD/2
I would like to know if the bias voltage of the RA and LA signals will become unstable.
Simply put, please comment if there is any problem with designing with RA & LA DC coupling with DC bias. - Another question is that in case of DC lead off function by applying DC coupling with DC bias,
there is a problem that it is recognized as lead-on even though it is lead-off status due to the pull up resistance connected to RA and LA for biasing. How can it be fixed?
TIA for your support.