This is our ouput value plot. Do we need to do calibration?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi! TCT:
This is our ECG data. X-Axis is ms. 80% main board's data just like this plot. Less 5% Y-Axis data would shift. The shift value is random. In our manufacturing process, we did not calibrate this sensor. Do we need to do calibration?
Hi Ariel,
The ADS1292R does not need any calibration to acquire the ECG signal. It doesn't look like you are getting the correct ECG signal from the hardware. I recommend using an ECG patient simulator to test your hardware or use the internal test signal function to ensure that the signal chain is working correctly.
Thanks
-TC
Hi! TCT:
Thanks your reply! This plot is using ECG patient simulator to send 2Hz sin wave.
There are 2 failed plot.
Plot_1 is total signal shift.

Plot_2 is signal distortion.

For now our engineer replaced the capacitance at Vref or replace ADS1292R to solve those 2 issue.