Part Number: ADS7038
Dear Team
Good day!
The ADS7038 datasheet shows the max for tCONV is 600ns.
What is the min for tCONV?
For example, if my tCYCLE is 1000ns and I need 600ns for acquiring the sample (tACQ) then could I make tCONV only 400ns?
Also, when I'm writing to registers like the GENERAL_CFG and SEQUENCE_CFG registers and I want to sample at 1MSPS
then do I still need to meet tCYCLE=1000ns during the register write or can it be 1800ns for example?
In other words can I use 1800ns to write to the GENERAL_CFG register then go back to tCYCLE=1000ns for my sampling and will everything be OK?
Thanks,
Leon.liu