Part Number: TLC5540
In the datasheet of TLC5540IPW, it is mentioned that "It is recommended to place the digital output data latch (if used) as close to the TLC5540 as possible to minimize capacitive loading. If D0 through D7 must drive large capacitive loads, internal ADC noise may be experienced.", but no where it is mentioned that what is the drive strength which output Data bit pins can support?
We are planning to use TLC5540IPW in our design in which we will be connecting the D0-D7 bits to Xylinx FPGA "XC4010E", so could you please confirm whether we can directly connect the Data lines to FPGA or is it a must to have a buffer in between?