Part Number: ADS1148-Q1
Other Parts Discussed in Thread: ADS1148, ADS114S06, ADS114S08, ADS1261-Q1, ADS1118-Q1, ADS1115-Q1, ADS1113-Q1, TMUX1308-Q1, ADS1114-Q1
Hi
We need a 16-bit high-precision ADC to collect the output signal of Hall sensor and achieve high-precision sampling requirements.
ADS1148-Q1 is a 16-bit ADC, and the ADS1148-Q1 channel is a differential or single-channel signal compatible mode.
If the use of single signal acquisition, single power supply, how to design the specific circuit?
If ADS1148-Q1 is used to collect the 6-way Hall sensor voltage signal, the signal input range is 0~5V.
So where does the commen input connect to?How to design?Is ADS1148-Q1 OK?Thank you very much!
Or please recommend a more suitable ADC, thank you!