This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: Is a Bode plot of the PGA frequency response available?

Part Number: ADS1298

Or put another way, can one assume the rolloff above the 3 dB down point (e.g. 32 kHz at G = 12) is that of a single order filter (6 dB/octave or 20 dB/decade)?