Other Parts Discussed in Thread: TLV320ADC6120, PCM6260-Q1, TLV320ADC6140
Dear:
can you promote a suitable part number,to support 6CH MIC input ADC (audio sampling),with echo eliminated function
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV320ADC6120, PCM6260-Q1, TLV320ADC6140
Dear:
can you promote a suitable part number,to support 6CH MIC input ADC (audio sampling),with echo eliminated function
Hello,
We are not going to have a 6-channel audio ADC solution with integrated Acoustic Echo Cancellation (AEC). We have a new popular family of Audio ADCs, the PCM6260-Q1 which are meant specifically for microphone acquisition with diagnostics and integrated low-noise MICBIAS boost signal. A combination of two TLV320ADC6140(4-ch) devices or a TLV320ADC6140 (4-ch)+TLV320ADC6120 (2-ch) would also work for 6 total channels with some higher performance options.
I mention them because even though they don't have any on-board DSP AEC processing they're very commonly used in 6-channel microphone systems with AEC and ANC type algorithms running on the host processor where more memory and MIPS are usually available for these acoustic algorithms.