Part Number: ADS7042
Hi,
based on the timing diagram (attached), ADS7042 cannot provide simultanesou sampling if there are multiple used with typical SPI. Is that correct?

I am looking for an ADC with similar characteristics, such as:
- 10-12 bits
- without need for external reference
- low power (up to 5mW)
- AVDD and DVDD can be at 1.8V
- Can allow simultaneous sampling with a timing diagram as the following.

Is there any available with the above mentioned characteristics?
Thanks!