Part Number: ADS1256EVM-PDK
Other Parts Discussed in Thread: ADCPRO, ADS1256
Hi,
Good day.
Our customer is using the ADS1256EVM-PDK and they have the following observations and question.
"I've purchased an ADS1256evm-pdk for evaluation of the mentioned ADC
And I'm trying to use the ADCPro software, but it is *very* buggy - do you have any information/resources on software that I can use to evaluate the EVM card
Typically errors in the DLLs / USB drivers
that's one of the messages. The software can sometimes not be closed and I need to reboot the computer.
This one is especially tricky...
And this one frequently occurs.
Quite often memory issues, do you have perhaps some issues with memory leakage and garbage collect in the code? After som time I am not able to capture only 100-sample sequences
I do see from the forums that I am not the only one with issues with the software. Is there a way to bypass the ADCPro and use e.g. python or so?
In general, is there a way to store the default settings, since I have to restart every five minutes or so, it takes some time to remember to program the chip with the settings. Like sending the entire register map or so?"
We appreciate your inputs and help on this matter. Thank you.
Regards,
Cedrick