Part Number: ADS131E06
Hi team,
My customer will use ADS131E06 for his application and he is adjusting timing of RESET after PoR.
Although he thought VCAP1 would be charged immediately after power-up of supplies, there is about 400ms delay for start of charging as this waveform(VCAP1.png) which can be accessed via TI internal network.
CH1: Power_EN
CH2:VCAP1
CH3:RESET
Please ignore 1st glitch of supplies/RESET. This is caused by instrument side.
Also, he will add additional 800ms delay for RESET from setup of the wavefrom.
Why start of VCAP1 charging shows delay?
Is it expected behavior?
Additionally, about 100mV voltage remains on VCAP1 even after power down.
Is this correct behavior(is this just matter of capacitor side)?
Best regards,
Shota Mago
Best regards,
Shota Mgo