Part Number: TSW14J56EVM
Other Parts Discussed in Thread: ADS54J60, ADS54J60EVM
Hi,
I have two queries:-
1) If I need two or more TSW14J56evms to run parallelly, do I need to just enable the trigger option in the HSDC software, or Is there some other code I need to change as well? And If I just need to enable the trigger option, then how can I capture the data if I want to provide the trigger again and again. Changing the settings everytime is not a viable option here.
2) I get the Clock message everytime I set the Sampling Rate; I have set ADS54J60_8224 device; clock- 983.04M (in ADSevm GUI); 8MHz input freq; 1.9Vpp; 50 ohms load. Can you tell me why am I receiving this message?

Thanks,
Raeleen