This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80508: Gain, Reference Divider, and Full-Scale Range

Part Number: DAC80508

Folks,

With reference to figure 36 in the datasheet

  • Reference = 2.5V

It would appear that a DAC code of 0x3FFF generates an output voltage of 5V.    If the Gain = 2, and reference divider = 1, shouldn't a full-scale code of 0xFFFF generate 5V.    I'm a little confused here.

Don