Hello,
I'm trying to bring up a circuit that includes a DAC60501M and I'm finding I get no output whatsoever. Relevant section of schematic below. From what I understand from the datasheet, the default settings should be sufficient to give an output as soon as the POR sequence is complete, and because I'm using the 'M' version it should go to midscale. I therefore expected that as soon as I applied 3V0_COND to the VDD pin, I would see midscale voltage at the output. It doesn't - it just sits at 0V. It doesn't respond when I try to write the DAC value register either, so I have to assume there's something fundamentally wrong that's preventing me seeing any output at all. It's a weird one as it the circuit design seems simple enough.
Intention is to operate in SPI mode by pulling pin 4 low. Verified that 3V0 is correctly being applied to pin 1 (VDD).
Because it should run in SPI mode, I can't read any registers which is a bit of a pain, but it seems so simple that I'm surprised there's any issue. Have I done something stupid here?
Thanks,
Gordon.