Hi Support team
My customer received a new pc Win10 based, and needs drivers for the 2014evm. Tried finding them on the web but links are broken
Can you point us to the correct locations?
Thanks
Jeff Coletti
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support team
My customer received a new pc Win10 based, and needs drivers for the 2014evm. Tried finding them on the web but links are broken
Can you point us to the correct locations?
Thanks
Jeff Coletti
Hi Jeff,
The drivers are no longer available due to having potential compatibility trouble with Windows 10 systems. I can provide the drivers but please note that there may be some trouble getting this working on a Win10 system.
TSC2014 EVM SW Installer W7.zip
Regards,
Aaron Estrada
Hi Jeff,
I would also like to include a .txt file with some instructions here.
TSC2014EVM Install Procedure To install the TSC2014EVM: 1. Go to the Installer directory, download the TSC2014EVMSWInstaller.zip to your PC. 2. Unzip the file and run setup.exe. 3. Accept the license agreement, and continue the installation. 4. Follow the instructions and prompts given. 5. When this completes, click Finish on the TSC2014EVM installer window. 6. Restart your computer. (This step may not be necessary, but is suggested as a precaution). 7. When your computer is restarted, connect the TSC2014EVM via a USB cable to the computer. Windows should recognize the new device, and "Found New Hardware Wizard" appears. 8. Select "Install from a list or specific location (Advanced)", and click on Next>. 9. Select "Don't Search. I will Choose the driver to install", and click on Next>. 10. If TSC2014EVM is inside the list of "Model", click on it to select it. you are done. 11. If it is not there, find and select NI-VISA USB Devices, 12. select "Browse ...", find the TSC2014EVM.inf, which is included with the install and located (by default) at: C:\Program Files\Texas Instruments\TSC2014EVM\data 13. click on and select it, and then click on "OK". 14. Your PC should show TSC2014EVM in the "Model" list now. Click on "Next". 15. you PC should install it. 16. click on Finish to finish the correction. 17. You are done! Run the TSC2014EVM software.
Regards,
Aaron Estrada