Part Number: DAC5578
Dear TI Team
There is the following description about Zero-code error. If you read this, is it correct to recognize that the Zero-code error changes depending on the output voltage?

Also, if the Zero-code error changes depending on the output voltage,
is it correct to recognize that it changes only 4 mV or less at the maximum according to the following rules?

Best Regards,
Y.Ottey