Part Number: ADS8684A
Hello everyone
I am using the ADS8684A in a system with a F28379D.
The F28379D is the SPI master and I can communicate with the ADS because I can read the program register as the range of the channel...
But when I try to read the value of the channels they are always at the maximum value even when I send nothing on the entry...
I send you my hardware config and my soft but do enyone has an idea about this ? Thank you in advance guys !
then if ret == 1 I start the auto rst mode by sending NO_OP command
Here is my hardware config
Again, thank you in advance...