This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4122: ADS4122

Part Number: ADS4122


Dear Ti support,

in the ADS4122 Datasheet it is suggested to select "mode 2" to enhance the performance for input frequencies above 230MHz (Register address = 4Ah, register data = 01h ).

What does this enhancement actually mean? what happens by selecting this mode? It would be great to get some hints for understanding, as this seems the only (possibly good, possibly not good) reason why we should change ADC configuration via SPI.

Thank you.

Best regards,

Paolo Castiglione

Digital Signal Processing Designer

 

paolo.castiglione@austrianaudio.com

T +43 1 934 6826 230

M +43 676 847490 230

 

AUSTRIAN AUDIO GmbH 

Eitnergasse 15 ● 1230 Vienna ● Austria

UID: ATU72389649 ● CRN: FN472051v

https://austrian.audio