Part Number: ADS1259
I am using A/D ADS1259.
* Operating voltage is +5 vdc and ground
*using internal reference +5.5 vdc
*using external power supply for input to IN+ and IN-
I am having problems reading in full scale from +5 to ground. It's like the A/D only reads half the range.
I am writing into the registers the following
Command 0x40, 0x08, 0x85,0x03, 0x17, 0x00,0x00,0x00, 0x00,0x00,0x40
What should the offset be? I have the gain set for gain factor of 1