Part Number: ADS131M06
Hi,
Can you please help me in understanding noise level lost in conversions?
I wanted to measure 300VAC with the resolution of 1V
how i will make sure that with this ADC, I will achieve this resolution.
Regards,
Deepak
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS131M06
Hi,
Can you please help me in understanding noise level lost in conversions?
I wanted to measure 300VAC with the resolution of 1V
how i will make sure that with this ADC, I will achieve this resolution.
Regards,
Deepak
Hello Deepak,
Thank you for your post and welcome to our forum.
1V / 300 Vac is approximately 50 dB of dynamic range: 20 x log10 (1 / 300). With the ADS131M06, you can achieve up to 102 dB at Gain = 1, or up to 80 dB at Gain = 64. Your input signal will have to be divided down to within the full-scale and absolute voltage ranges of the ADS131M06.
Regards,
Ryan
Of course, technically then it is 20*log(300/1). We generally speak of dynamic range in absolute terms to describe the difference between two magnitudes: the largest and smallest signals measured by the system.
You can validate the noise performance of the device by shorting the input pins together and biasing them to a mid-supply common-mode. The results of the peak-to-peak and RMS noise that you measure will be very close to the data presented in the Noise Measurements table in the data sheet.
Regards,
Hi Ryan,
Got it..
I have designed circuit already with with 91k (Upper) and 1k (bottom)
Now i wanted to measure noise floor with the data that i have processed via UART.
How i will come to conclusion that we are achieving resolution of 1V
Hi Deepak,
A change of 1 V in your input signal will produce a change of 10.9 mV at the ADC input using the resistor divider circuit you described. This is much better than the resolution of the ADS131M06.
Regards,
Ryan