Other Parts Discussed in Thread: DAC5682Z, CDCM7005
Hello,
I am using the TSW3100 to generate a single sinusodial tone with 50MHz
via the DAC5682Z Evaluation Module. I use the multitone software
(version 1.0) which was delivered with the TSW3100 board to generate
this signal, and an external clock signal of 1GHz, 13 dBm (1 Vrms for 50
Ohm). For the DAC Board settings, I utilized the sample configuration
files delivered with the software: Example_2.reg7005 for CDCM7005 and
Example_2.reg5682 for the DAC6582Z (single DAC, 2x interpolation). The
board is in its default configuration (jumpers) and the only thing I
have changed are the 4 resistors you need to uninstall (R137, R156,
R153, R155) and I installed R134, R109, R155, R156 instead to measure
directly the DAC output without the modulator. The transformers are not
shortened. When I measure the output signal, I obtain a sine around 6
MHz exhibiting a lot of harmonic distortion, on both outputs IoutA2 and
IoutB2. I attached the register files and screen shots of the signal I
measured and screenshots of the settings I used for the multitone software
and for the DAC6582Z software. It would be great, if someone had an idea
what is going wrong with my settings.
Also, is it possible to get the latest version of the multitone pattern
generator software?
Best regards,
Michael Soudan