Part Number: ADS1220EVM
Other Parts Discussed in Thread: ADS1220
In the ADS1220EVM, there is a U2 whose part number is SN74LVC2G157DCTR, I want to know the U2 function in the circuit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1220EVM
Other Parts Discussed in Thread: ADS1220
In the ADS1220EVM, there is a U2 whose part number is SN74LVC2G157DCTR, I want to know the U2 function in the circuit.
Hi Vast,
U2 is a 2-input mux to allow a provision for an external clock to the ADS1220. The default is for the CLK pin to be set low for use of the internal oscillator of the ADS1220 to be used as the clock source. U2 is not needed in normal operation. Either an external clock will be supplied directly to the ADS1220 CLK pin or the CLK pin will be grounded to use the internal oscillator.
Best regards,
Bob B