Hi,
I am designing a board where an ADS6144 will be connected to a Cyclone 10GX FPGA. This FPGA (like many newer devices) does not have many 3V tolerant pins. I would like to use the LVDS interface of the ADS6144 and connect it to the 1.8V I/O domain of the FPGA. I would also like to configure the ADC using its serial port rather than pin-strapping, because I want to use the test data features of the ADC. This should be fine, but I worry that a one bit programming error in the selection of the output mode could cause the output to enter CMOS mode and destroy the input buffers of the FPGA. Is there anyway to force the part into LVDS mode while still using serial configuration?
Cheers, Mark