Part Number: ADS1220
Hi team,
My customer considers to use ADS1220 and he is asking a question about input range.
He would like to measure single-ended 0~5V analog input with usage of AVDD-AVSS=5V, VREFP0-VREN0=5V.
Before the register is written to set external reference mode, there is possibility that up to 5V will be applied to input(AIN0) while AIN1 is shorted to GND.
It exceeds default internal reference voltage(2.048V).
Even though input range exceeds default internal reference voltage, it doesn't damage the device as long as input voltage is below AVDD.
Is this understanding correct?
Best regards,
Shota Mago