Other Parts Discussed in Thread: DAC1282, ADS1282, DAC9881
Hello,
I was over in: http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/303479/1059565.aspx#1059565 and it was suggested I ask the question in a couple of the other forums.
You can refer to the above link for background - question is achieving 24-bit resolution and accuracy for a control loop - in this case for an EFC for an OCXO.
Is there a low-speed Audio DAC that would work? In the past the Burr-Brown PCM61P was used in this design - that was only 18bits but that design had a manual pot also for that reason I suppose.
I have looked at the available DACs - some are nice in that they have a glueless interface to the 28069 (McBSP) - but is it a good way to control a noise sensitive circuit like an EFC for an OCXO?
I realize TI has a 24-bit DAC for seismic applications - the output is differential. If I tried that in this application I would have to convert the output to single ended - and that part is currently pricey. But maybe that is the best approach.
Alternatives are PWM (don't think the real bit resolution can be 24 with the 28069) and putting two 16-bit DACs together with the proper weighting for the resistors through a summing op-amp.
I should add that the output voltage should be a held DC mode like the DAC1282 has.
Suggestion appreciated.
Thanks,
johnw