Other Parts Discussed in Thread: ADS1298, ADS1298R
Hi,
I'm doing a research project about bioamplifiers and chose the ADS1298.
As a first step, I made a breakout board to access the pins and connected them to an Arduino, a breadboard and the development board as a power supply, but I'm not able read the chip's ID.
I use the Arduino for the SPI communication and as a power supply for the development board, which I use again in order to provide a biopolar supply for the chip on the breakout board.
I also installed the VCAPs. I tested my Arduino code with the development board and it works.
There is a schematic, a picture of the setup and the Arduino code attached.
Is there something wrong with the wiring? Or could it be, that the chip is broken?
Thanks for any help
Dominik
#include <SPI.h>
void setup(){
pinMode(4, OUTPUT);
SPI.begin();
SPI.setBitOrder(MSBFIRST);
SPI.setDataMode(SPI_MODE1);
adc_send_command(0x11);
delay(500);
}
void loop()
{
delay(500);
Serial.begin(115200);
int ID = 1;
digitalWrite(4, LOW);
SPI.transfer(0x20);
delayMicroseconds(5);
SPI.transfer(0);
delayMicroseconds(5);
ID = SPI.transfer(0);
delayMicroseconds(1);
digitalWrite(4, HIGH);
Serial.println(ID);
}
void adc_send_command(int cmd)
{
digitalWrite(4, LOW);
SPI.transfer(cmd);
delayMicroseconds(1);
digitalWrite(4, HIGH);
}