Hello,
For ADS1299 internal input short condition, which both inputs of PGA be (ADSS+AVDD)/2 by setting register value MUX[2:0],
As seen below, I'm getting ~1uV on ADS1299 EVM with power supply in bi-polar (+-2.5V).
And, corresponding register settings are,
However, on our developed board with same exact register setting as above, I'm getting ~20uV of noise level.
[Raw data plot is attached below] I believe it picks up ECG pretty successfully, but not EEG. (guess it's due to high noise level).
I think we met pretty much all the PCB design criteria / requirements for successful EEG signal acquisition, but I have no idea where does that amount of noise is coming from ?
On page 3. of ADS1299 Data sheet, Offset error is specified as 60uV. I wonder if that 20uV can be the offset error.
Then, Does ADS1299 EVM plots raw data without offset ?
Can anyone comment on this ? Thank you.