This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84EVM: FIFO read error

Part Number: DAC38J84EVM
Other Parts Discussed in Thread: DAC38J84, , LMK04828

Hello everybody,
I have some questions about interfacing with the DAC38J84.I hope you can help me or give some advice.

I am trying to interface the DAC38J84EVM board and the Xilinx KC705 FPGA using the JESD204b interface. I am using the onboard LMK clock for JESD and FPGA clock generation.
The logical FPGA core is transmitting data and SYNC is asserted, after triggering SYSREF, but i always get 'FIFO read error' and 'FIFO read empty' high, even after clearing and reading them when the link is established. No data is output from any of the DACs.

I tested the DAC with the internal NCO and can confirm normal operation.
Can this be a problem with the initialization sequence?

The JESD parameters are as follows:

FPGA: Xilinx K705 using Xilinx JESD204B IP core
L=4, M=4, F=2, K=10, S=1, HD=0
DAC input rate: 122.8 MSPS
interpolation: 2
FPGA ref = FPGA core clk = 245.76 MHz

Also attaching the DAC config file.

Hoping for some help

Thank you,

Ignas

LMK04828 
0x00 0x00
0x02 0x00
0x100 0x18
0x101 0x55
0x103 0x01
0x104 0x20
0x105 0x00
0x106 0xF0
0x107 0x11
0x108 0x63
0x109 0x55
0x10B 0x01
0x10C 0x20
0x10D 0x00
0x10E 0xF0
0x10F 0x76
0x110 0x08
0x111 0x55
0x113 0x00
0x114 0x00
0x115 0x00
0x116 0xF9
0x117 0x00
0x118 0x18
0x119 0x55
0x11B 0x00
0x11C 0x20
0x11D 0x00
0x11E 0xF9
0x11F 0x00
0x120 0x10
0x121 0x55
0x123 0x00
0x124 0x00
0x125 0x00
0x126 0xF9
0x127 0x11
0x128 0x08
0x129 0x55
0x12B 0x00
0x12C 0x00
0x12D 0x00
0x12E 0xF9
0x12F 0x00
0x130 0x08
0x131 0x55
0x133 0x00
0x134 0x20
0x135 0x00
0x136 0xF9
0x137 0x01
0x138 0x00
0x139 0x02
0x13A 0x00
0x13B 0xA0
0x13C 0x00
0x13D 0x08
0x13E 0x03
0x13F 0x00
0x140 0x00
0x141 0x00
0x142 0x00
0x143 0x12
0x144 0xFF
0x145 0x00
0x146 0x10
0x147 0x1A
0x148 0x02
0x149 0x42
0x14A 0x02
0x14B 0x16
0x14C 0x00
0x14D 0x00
0x14E 0xC0
0x14F 0x7F
0x150 0x03
0x151 0x02
0x152 0x00
0x153 0x00
0x154 0x78
0x155 0x00
0x156 0x7D
0x157 0x00
0x158 0x96
0x159 0x06
0x15A 0x00
0x15B 0xD4
0x15C 0x20
0x15D 0x00
0x15E 0x00
0x15F 0x0B
0x160 0x00
0x161 0x01
0x162 0x44
0x163 0x00
0x164 0x00
0x165 0x08
0x166 0x00
0x167 0x00
0x168 0x08
0x169 0x59
0x16A 0x20
0x16B 0x00
0x16C 0x00
0x16D 0x00
0x16E 0x13
0x17C 0x15
0x17D 0x0F
DAC_RESET 
0x00 0x1
DAC3XJ8X 
0x00 0x0118
0x01 0x0003
0x02 0x2002
0x03 0xA300
0x04 0xF0F0
0x05 0xFF07
0x06 0xFFFF
0x07 0x2C00
0x08 0x0000
0x09 0x0000
0x0A 0x0000
0x0B 0x0000
0x0C 0x0400
0x0D 0x0400
0x0E 0x0400
0x0F 0x0400
0x10 0x0000
0x11 0x0000
0x12 0x0000
0x13 0x0000
0x14 0x0000
0x15 0x0000
0x16 0x0000
0x17 0x0000
0x18 0x0000
0x19 0x0000
0x1A 0x0000
0x1B 0x0000
0x1E 0x9999
0x1F 0x9980
0x20 0x8008
0x22 0x1B1B
0x23 0x01FF
0x24 0x0020
0x25 0x2000
0x26 0x0000
0x2D 0x0001
0x2E 0xFFFF
0x2F 0x0004
0x30 0x0000
0x31 0x0400
0x32 0x0000
0x33 0x0000
0x34 0x0000
0x3B 0x0000
0x3C 0x0028
0x3D 0x0088
0x3E 0x0128
0x3F 0x0000
0x46 0x1882
0x47 0x01C8
0x48 0x3143
0x49 0x0000
0x4A 0x0F01
0x4B 0x0801
0x4C 0x0903
0x4D 0x0300
0x4E 0x0F0F
0x4F 0x1C61
0x50 0x0000
0x51 0x00DC
0x52 0x00FF
0x53 0x0000
0x54 0x00FC
0x55 0x00FF
0x56 0x0000
0x57 0x00FF
0x58 0x00FF
0x59 0x0000
0x5A 0x00FF
0x5B 0x00FF
0x5C 0x1133
0x5E 0x0000
0x5F 0x3210
0x60 0x5764
0x61 0x0211
0x64 0x0003
0x65 0x0003
0x66 0x0003
0x67 0x0003
0x68 0x3D0F
0x69 0xFF0E
0x6A 0xD50B
0x6B 0x190E
0x6C 0xF007
0x6D 0x0060
0x6E 0x0000
0x6F 0x0000
0x70 0x0000
0x71 0x0000
0x72 0x0000
0x73 0x0000
0x74 0x0000
0x75 0x0000
0x76 0x0000
0x77 0x0000
0x78 0x0000
0x79 0x0000
0x7A 0x0000
0x7B 0x0000
0x7C 0x0000
0x7D 0x0000

  • DAC38J84_442_122.88.pptxIgnas,

    I got your settings working with our setup using the DAC38J84EVM, TSW14J10EVM, and a KC705. See if the settings in the attached file help you.

    Regards,

    Jim

  • Hello Jim,
    I am not using the TSW14J10 and trying to interface directly. I replicated the settings as shown in the file, but with divider values set to CLKout0,1 -12, CLKout2,3 – 12 and CLKout12,13 – 12, I still get FIFO empty (SYNC is ok).
    If I try setting CLKout0,1 to 24, I don't get the FIFO empty error and can observe some data on the output, but I get 8b/10b disparity errors and get no SYNC. What could be the cause of this? The IP core is configured with a reference of 245.76MHz and line rate of 2.4576Gbps. Could this be the problem of different SerDes linerates in the transmitter and receiver? Is there a register in the DAC or LMK which specifies SerDes linerate? How is it calculated?
    Thank You
    Ignas
  • Ignas,

    There are no registers that tell you what the line rate is. See the attachment for how you would calculate the line rate.

    Regards,

    Jim

     DAC Line rate calculation.pptx

  • Jim,

    I got my DAC working. The problem was the Xilinx IP core in the FPGA.  Xilinx JESD IP coreclk must be set to 1/40 of the SerDes linerate, therefore not all DAC settings can be used.

    Got mine working with the following procedure, should anybody find it useful:

    In the DAC3XJ8X configuration GUI Quick start tab:
    1.    Select EVM Clock Mode – onboard
    2.    DAC data input rate – 245.76 MSPS
    3.    Number of lanes – 4
    4.    Interpolation – 1
    5.    Press “Program LMK  and DAC” button and wait for it to finish

    In the LMK04828 controls tab:
    1.    Set DCLK Divider to 24
    2.    Deselect CLKout 12 and 13 Group Powerdown


    Programming and reset of the TX core:
    1.    Program or reset the FPGA


    Back at the quick start tab:
    1.    Press the Reset DAC JESD core button
    2.    Press Trigger SYSREF button

    After configuration, press Clear Alarms and Read in the Alarms and Errors tab. No errors should be present in the enabled RX lanes.

    Thanks for the help

  • Ignas,

    Glad to hear this. Thanks for the feedback.

    Jim