Part Number: ADS1293EVM
Other Parts Discussed in Thread: ADS1293,
Have anyone performed IEC 60601-2-47 test item 201.12.4.4.102?
It is used to check device input impedance.
It first check 5mV 10Hz sinusoidal signal, then adding a 620K ohm resistor between input and ADS 1293EVM board.
By checking the Vpp of output signal, input impedance can be calculated from the variance of Vpp of sinusoidal signal.
When I do this test, it is found no output signal (or weak , 10-30uV). Is it right behavior?
Regards,
Yuan Te Liu