This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J60: DC-coupling with offset

Part Number: ADS54J60


ADS54J60 supports DC-coupling with offset

Hi,

Let me question whether the analog input of the ADS54J60 supports DC-Coupling.

We attach circuit configuration, input waveform, output data diagram.
Connect the +IN terminal of the differential amplifier to GND,
Input the signal to the -IN terminal.
For VOCM of the differential amplifier, input 2.0V from 22pin (VCM) of the ADS54J60.

We gave the following two types of inputs and confirmed the AD-conversion data.

case1
Connect a 50Ω resistor to the -IN terminal of the differential amplifier and input 0V.
Make sure -OUT and + OUT of the differential amplifier are both 2.0V (VCM voltage).
The result of A / D conversion for 0V has no problem.

case2
Input the DC-voltage (for example 200mV) to the -IN terminal of the differential amplifier.
A DC-offset voltage is applied to VCM at -OUT and + OUT of the differential amplifier.
The voltage is input to the ADS54J60.
The result of AD conversion at that time does not become DC-voltage.
A waveform like the attached waveform is output.


Question1
Is the analog input of the ADS54J60 compatible with DC-Coupling?
(Input offset voltage is several hundred mV)

Question2
When DC-coupling is possible, is it necessary to input a signal with 2.0V as common to the analog input terminal?

If DC-Coupling is not possible if an offset of several hundred mV is applied to the signal,
It is also possible to change to AC-Coupling.

best regards