Part Number: ADS1282
Other Parts Discussed in Thread: ADS1283
Hi Chris,
We are using the ADS1282 in a single channel wireless seismic data acquisition system that is synchronized to GPS. Each data acquisition box has a GPS receiver and an ADS1282 and the ADS1282 is synchronized on the leading edge of the GPS 1 PPS signal after lock is achieved. We occasionally see timing errors in the data ranging from one sample to 16 samples or more. There is currently no provision to synchronize the SYNC signal to the CLK.
In a recent post on ADS1282 Synchronization, you indicated that the SYNC signal needed to stay at least 30ns away from the rising edge of the CLK. What range of errors would one be likely to see if the SYNC signal sometimes violates the CLK setup and hold timing?
You suggested toggling SYNC pin twice, (low-high-low-high). How fast or slow does this toggling have to be? For example, with SYNC initially low, would raising SYNC for 1us and then lowering it for 1us and then setting and leaving it high be sufficient?
- Kent