This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300 SPI read write issue

Part Number: AFE4300

I have a problem in getting the ti AFE4300 start the ADC measurement. I started with a new board that was designed using reference design on TI. Am trying to communicate with the board through an stm32f103rbt6.

I was set up spi mode 1 and want to use body composition measurement (BCM).

I give 1mHz to afe 4300 board by arm pwm signal.

These are what has happened

1. I can not read ADC data result register. 

2. the RDY pin status unchanged. it keep high status.

 

 

int main()
{
SystemInit();
UART2_Init();
DelayInit();
PWM_Init();



RESET_init();
init_spi1();

resetAFE4300();
initAFE4300();
initBCM();

//
while(1)
{


if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 1){

printf("register_Name\n\r");
printf("0x%X\n\r",readRegister(ADC_DATA_RESULT));
printf("0x%X\n\r",readRegister(ADC_CONTROL_REGISTER));
printf("0x%X\n\r",readRegister(MISC1_REGISTER));
printf("0x%X\n\r",readRegister(MISC2_REGISTER));
printf("0x%X\n\r",readRegister(DEVICE_CONTROL_1));
printf("0x%X\n\r",readRegister(ISW_MATRIX));
printf("0x%X\n\r",readRegister(VSW_MATRIX));
printf("0x%X\n\r",readRegister(IQ_MODE_ENABLE));
printf("0x%X\n\r",readRegister(WEIGHT_SCALE_CONTROL));
printf("0x%X\n\r",readRegister(BCM_DAC_FREQ));
printf("0x%X\n\r",readRegister(DEVICE_CONTROL_2));
printf("0x%X\n\r",readRegister(ADC_CONTROL_REGISTER_2));
printf("0x%X\n\r",readRegister(MISC3_REGISTER));

}
else if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 0){
//printf("%0x\n\r",readRegister(ADC_DATA_RESULT));
printf("low\n\r");
}
DelayMs(100);
}
}

void RESET_init(void){
GPIO_InitTypeDef GPIO_InitStructure;

//GPIO_PinRemapConfig(GPIO_Remap_SWJ_NoJTRST, ENABLE);
//GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);

/* Enable the GPIO Clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);

/* Configure the GPIO pin */
GPIO_InitStructure.GPIO_Pin = PIN_RESET;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure); 

GPIO_InitStructure.GPIO_Pin = SPI_CS_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = PIN_DRDY;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
//
GPIO_SetBits(GPIOA, GPIO_Pin_4);
}

uint32_t RDY_read(void){
return GPIO_ReadInputDataBit(GPIOC,PIN_DRDY);
}

void RESET_HIGH(void){
//GPIOA->BSRR = PIN_RESET; 
GPIO_SetBits(GPIOC,PIN_RESET);
}

void RESET_LOW(void){
//GPIOA->BRR = PIN_RESET; 

GPIO_ResetBits(GPIOC,PIN_RESET);
}

void resetAFE4300(void){
RESET_LOW();
//printf("111");
DelayMs(100);
RESET_HIGH();
}


void init_spi1(void){ // for MASTER mode
GPIO_InitTypeDef GPIO_InitStructure;
SPI_InitTypeDef SPI_InitStructure;
// GPIO_StructInit (& GPIO_InitStructure);
// SPI_StructInit (& SPI_InitStructure);

/* Enable GPIOs clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

/* Enable SPI clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

/* Configure SPI SCK pin */ 
GPIO_InitStructure.GPIO_Pin = SPI_SCK_PIN | SPI_MOSI_PIN | SPI_MISO_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);


/* SPI configuration -------------------------------------------------------*/

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; //32
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI1, &SPI_InitStructure);

/* Enable SPI */
SPI_Cmd(SPI1, ENABLE);

}

void writeRegister(unsigned char address, unsigned int data){
unsigned char firstByte = (unsigned char)(data >> 8);
unsigned char secondByte = (unsigned char)data; 

GPIO_ResetBits(GPIOA, GPIO_Pin_4);

SPI_SendByte(address);

SPI_SendByte(firstByte);
SPI_SendByte(secondByte);

GPIO_SetBits(GPIOA, GPIO_Pin_4);
}

int readRegister(unsigned char address){

int spiReceive = 0;
uint8_t spiReceiveFirst = 0;
uint8_t spiReceiveSecond = 0;

address = address & 0x1F; //Last 5 bits specify address
address = address | 0x20; //First 3 bits need to be 001 for read opcode

GPIO_ResetBits(GPIOA, GPIO_Pin_4); 

SPI_SendByte(address);
spiReceiveFirst = SPI_SendByte(0x00);
spiReceiveSecond = SPI_SendByte(0x00);

GPIO_SetBits(GPIOA, GPIO_Pin_4);

spiReceive = (spiReceiveFirst << 8);
spiReceive |= spiReceiveSecond;

return spiReceive;
}


void initAFE4300(void)
{
writeRegister(ADC_CONTROL_REGISTER,0x5140);
writeRegister(MISC1_REGISTER,0x0000); //
writeRegister(MISC2_REGISTER,0xFFFF); //
writeRegister(DEVICE_CONTROL_1,0x0004); //Power down both signal chains
writeRegister(ISW_MATRIX,0x0000);
writeRegister(VSW_MATRIX,0x0000);
writeRegister(IQ_MODE_ENABLE,0x0000); //
writeRegister(WEIGHT_SCALE_CONTROL,0x0000);
writeRegister(BCM_DAC_FREQ,0x0040); //
writeRegister(DEVICE_CONTROL_2,0x0000);
writeRegister(ADC_CONTROL_REGISTER_2,0x0011);
writeRegister(MISC3_REGISTER,0x00C0);
}

void initBCM(void)
{
writeRegister(ADC_CONTROL_REGISTER,0x4120); //Differential measurement mode, 32 SPS //4120//C1A0
writeRegister(DEVICE_CONTROL_1,0x0006); //Power up BCM signal chain
writeRegister(ISW_MATRIX,0x0408); //Channels IOUTP1 and IOUTN0
writeRegister(VSW_MATRIX,0x0408); //Channels VSENSEP1 and VSENSEN0
writeRegister(ADC_CONTROL_REGISTER_2,0x0063); //ADC selects output of BCM-I output
writeRegister(WEIGHT_SCALE_CONTROL,0x0000); //Gain = 1 DAC Offset = 0 0x603F
writeRegister(BCM_DAC_FREQ,0x0032);
writeRegister(MISC3_REGISTER,0x0030);
}

uint8_t SPI_SendByte(uint8_t Data)
{
while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI1, Data); 
while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);

return SPI_I2S_ReceiveData(SPI1);
}

Any leads would be of great help

  • Hello Ram,

    This is a duplicate post.
    Refer here e2e.ti.com/.../665268 for resolution.
  • I am facing the problem while using AFE 4300 .i have intialize the bcm with below configuration

    void initBCM(void)
    {
    writeRegister(ADC_CONTROL_REGISTER,0x4120); //Differential measurement mode, 32 SPS //4120//C1A0
    writeRegister(DEVICE_CONTROL_1,0x0006); //Power up BCM signal chain
    writeRegister(ISW_MATRIX,0x0408); //Channels IOUTP1 and IOUTN0
    writeRegister(VSW_MATRIX,0x0408); //Channels VSENSEP1 and VSENSEN0
    writeRegister(ADC_CONTROL_REGISTER_2,0x0063); //ADC selects output of BCM-I output
    writeRegister(WEIGHT_SCALE_CONTROL,0x0000); //Gain = 1 DAC Offset = 0 0x603F
    writeRegister(BCM_DAC_FREQ,0x0032);
    writeRegister(MISC3_REGISTER,0x0030);

    }

    void initAFE4300(void)
    {

    writeRegister(ADC_CONTROL_REGISTER,0x5140);
    writeRegister(MISC1_REGISTER,0x0000); //
    writeRegister(MISC2_REGISTER,0xFFFF); //
    writeRegister(DEVICE_CONTROL_1,0x0004); //Power down both signal chains
    writeRegister(ISW_MATRIX,0x0000);
    writeRegister(VSW_MATRIX,0x0000);
    writeRegister(IQ_MODE_ENABLE,0x0000); //
    writeRegister(WEIGHT_SCALE_CONTROL,0x0000);
    writeRegister(BCM_DAC_FREQ,0x0040); //
    writeRegister(DEVICE_CONTROL_2,0x0000);
    writeRegister(ADC_CONTROL_REGISTER_2,0x0011);
    writeRegister(MISC3_REGISTER,0x00C0);



    }

    if(adc_flag)
    {
    adc_flag=0;
    data1=readRegister(ADC_DATA_RESULT);

    }

    i am getting wrong adc value which is fluctuating from 21930 to 43945.

    and i have connected 1K register Between IOUT1 (26)and  IOUT0(27).

    please Suggest me where i am going to wrong.

    Regards

    Ram

  • Hello Ram,

    I am assuming you were able to figure out the issue with your code and setup.
    I am closing the thread now.
    Please let us know if you have any further questions.
  • Thanks for late response .I have not get any solution from you. I am still waiting for solution 

  • Hi Ram,

    One thing to check is how is the measurement in FWR mode as compared to IQ mode.
    This will give the idea about the setup related issue.

    Regards,
    Prabin
  • Hi Ram,

    I assume your questions have been answered and so I will close this thread.
    Please start a new thread if you have any further questions.