Part Number: ADS1298R
Hello! Section 9.3.1.7.8.2 of ADS1298R datasheet describes:
When this respiration option is enabled, ADS129xR channel 1 cannot be used to acquire ECG signals. If the RA and LA leads are intended to measure respiration and ECG signals, wire the two leads into channel 1 for respiration and channel 2 for ECG signals.
So:
1) is it possible to wire the two leads (RA and LL) into channel 1 for respiration and channel N != 1 (for example 6) for ECG signals?
2) is it possible to connect leads RA and LL to some else inputs while ones already connected to IN6 and RES circuit?