Part Number: ADS1298RECGFE-PDK
Other Parts Discussed in Thread: ADS1298R
Hello,
I am using the ADS1298RECGFE PDK (Rev B.) with the MMB0 controller currently. Since it is connected to the MMB0 board using berg sticks and is removable, I wanted to use it with an MCU development board for SPI evaluation. What is the procedure to use this board as a breakout. Do I make the connections directly using the jumpers on the daughter board? Or do I need to use the pinouts from the same? Is there any documentation available for making these connections?