This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5562: Use ADS5562 with LMH6552

Part Number: ADS5562

Hi. 

I am reading the data sheet.

Look at Figure 60 on page 46 of the data sheet.

Can I supply 1.5V voltage source (IN+) and 1.5V DC?

  • Hi User,

    Yes, with the VCM of +1.5V, and voltage rails of +5V/-5V, providing a 1.5V signal should not be an issue. Is this an AC input or DC input to the ADC?

    Best Regards,

    Dan

  • Hi dBrock. Thank you for reply my answer.

    Did you mean the 1.5V (in red circle) is DC voltage?

    I will supply AC voltage to Vin. (VCM ± 0.9V).



  • Hi User,

    Yes, this is what I meant, but was asking if you are supplying an AC or DC signal to the LMH5552 beside the 1.5VCM (you already answered).

    Best Regards,

    Dan