Part Number: ADS127L01EVM
Other Parts Discussed in Thread: LMK00804
Dear Sirs,
With the board I used ADS127L01EVM, I am measuring the analog differential voltage signal from a gyro. I want to send my digital data to another MCU (TM4C1294XL), but the receiving side has a 16-bit RX FIFO. Therefore, it can not read 32-bit SPI data from the ADS127L01EVM.
While converting 24 bit analog Gyro data to digital data, I want to send it countinously to a proper MCU for filtering or some math operations. MCU will process and send the data by using CAN or another communication channel.
Measured signals on oscilloscope screen where the signal designations are as follows:
Pink: DOUT
Yellow: CLK
Blue: FSYNC
Mode: Frame-sync master mode
WB2 , OSR 256
ADS127L01EVM works fine but the SPI output is 32 bit. My MCU has max. of 16 bit RX FIFO.
We opened a question with the Other microcontrollers forum. I have confirmed that the two cards are incompatible.
Would you have any recommended MCUs compatible to work with ADS127L01EVM to recieve 32-bit data from the ADC we are currently using?
Do you recommend a compatible MCU for ADS127L01EVM ? Because the ADC has 32 bit SPI transaction.
You may advice me to use another ADC board compatible with my TM4C1294XL.
Regards,
Riza