Hello, I would like to connect 3 ADS1299 to 1 SPI protocol, it is poss ible? Please, see the picture, is it the correct connection?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I would like to connect 3 ADS1299 to 1 SPI protocol, it is poss ible? Please, see the picture, is it the correct connection?
Hello Michail,
Welcome to TI E2E forum!
Please refer to section 10.1.4 in the ADS1299 datasheet for multiple device configuration.
You cannot short the DRDY output together since it is not open drain output.
If you keep the device synchronized by using the START signal (refer figure 69), then you can use one DRDY signal from one of the devices as the data ready interrupt to the processor.
Hello Michail,
This configuration looks fine.
Please ensure the CLK signals across the devices are also synchronized.